Part Number: LMP2012QML-SP
I am looking into the possibility of using "LMP2012QML-SP" as a temperature switch (e.g., below 1 temperature it has 1 output, and above that temperature it has a different output). However, I am having trouble understanding if this switch is "Single Pole Double Throw" or different? or would it behave as a simple single pole single throw switch? or I am having trouble understanding if I can use it as a switch at all? I see that the part has 10 terminals