This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC3301: Input locks up when powering up the amplifier

Part Number: AMC3301

Hi,

we used the AMC3301 to read low voltage source(5mV to 50mV) (chemical reaction sensor), but the input of the amplifier has to low impedance and our voltage source collapsed. Now we added a op amp (gain of 1) as a voltage buffer in front of AMC3301 input and with a separate power supply. When we connect everything up and do not power the AMC3301, we measure 5 to 50mV on the INP and INN of the amplifier. But once the AMC3301 is powered up (3.1V) the input locks to 87mV and doesn't move either way.

What could cause this?