Part Number: OPA325
Other Parts Discussed in Thread: OPA397,
Hi there,
sometimes datasheets report several values for a single parameter acquired using different test conditions, e.g., the parameter is measured using different temperature ranges.
One expects that the max. value of a parameter rises when the temperature range is extended, see here for example the input bias of OPA397:

This is not the case with the OPA325

These values seem not logical. I expect the test that applies a larger temperature range to report a max. value that is at least as big as a test that applied a subset of that temperature range.
How can the max value of IB decrease when the temperature range applied in the test increases?
Thanks.
Dan