Part Number: OPA454
Other Parts Discussed in Thread: OPA462, OPA455, OPA452, OPA828
Hi,
We have selected OPAMPs that meet the following requirements.
・ Voltage ± 50V (sine wave)
・ Current 350mA (Peak to Peak)
・ Frequency 300kHz ~ 400kHz
・ Load piezo element (capacitive load_1.5 μF)
I refer to the following circuit described in the DS of OPA454.
Is it possible to drive a load capacity of 1.5uF?
Best regards,
Hiroshi