Part Number: AMC3302-Q1
Other Parts Discussed in Thread: AMC3302
There’re several questions shown as below:
- The maximum current of battery pack is above 1100A while the current shunt resistor used is 50uΩ. Howerver, the maximum input of AMC3302-Q1 is only ±50mV, which does not meet the demand(<60mV).
- What would happen if the input voltage exceeds the maximum ratings(±50mV)?
- How can we evaluate the system measuring error usually?