Part Number: AMC3301
Other Parts Discussed in Thread: OPA2317, , AMC1301, AMC3330
Could there be any issue with a midpoint divider then unity gain buffer like I have drawn here? This schematic was originally drawn for the AMC1301, and I'd like to convert this to use the AMC3301 instead, using something like the OPA2317 as a unity gain buffer.
The probe in this design consists of a 2k shunt in a galvanic o2 sensor, so this precludes direct connection. The output range is 0-200mv dc.
With only 1ma usable external power, this doesn't leave a lot of good options for midpoint buffering. The datasheet shows connecting HGND to the negative side of the shunt, I assume this is only to keep the common mode input range correct.
The AMC3330 has no stock or I'd have used that part.
Any comments or suggestions?