Part Number: OPA858DSGEVM
Other Parts Discussed in Thread: OPA858,
Hi there,
I acknowledge that this may seem like an obvious question but I was wondering if I could get assistance with testing out the OPA858 amplifier as a Transimpedance amplifier. I was wondering if I could get assistance with the correct configuration for using the evaluation board as a TIA amplifier. I am working on verifying a PCB board with multiple circuits, one of which is based off of the OPA858DSGEVM evaluation board, which I am also testing at the moment.
I have been testing it with the default configuration and I am getting serious attenuation on any input frequency signal of 100 MHz or higher (ideally want to run it at 3-5GHz).
Thank you