Part Number: LMH2832
There seems to be limitations on the transient generator and number of parameters to control amplitude and phase coefficients! The program archive attached can not set all the generator frequencies with a variable and looking at the spectrum there is an error in the FFT plot which does not make sense
The time domain plot looks OK at least represents more than 3 harmonics! The harmonics generated are well inside the capability of the LMH2832 to mimic the source spectrum
The FFT plot is missing information - if I replace the frequency variable with a real value I can get the correct spectrum - so there seems to be a bug.
I need to control amplitude and phase of all the generators and the bug appears preventing the tool from correct measurements?
Notice the first generator is picking up the fundamental frequency OK but only the 4th harmonic (real number) is able to pass in the simulation!
How can this be fixed and what is the reason for the missing spectrum if it is a user error - it would be nice to know? Can anyone advise?
Bob