This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9154: AI and AO application

Part Number: TLV9154


We'd like to promote this TLV9154 for the AI and AO application in MD system. It has Rail-to-Rail input/output, and C-M range beyond both rails as (V-)-0.1V and (V+)+0.1V 

Operation Conditions:

VCC+=12V,typ, VCC-=0V (Single Power)

Analog Input voltage: 0V to 10V

Analog Output Voltage: 0V to 10V

Signal Frequency:100KHz

Is TLV9154 a best part to implement this AI/AO function? Or what parts you suggest? Why? thanks. 

Regards

Brian W

  • Hi Brian,

    The TLV9154 sounds like it would be a good fit in this application based on your requirements! But if you can give me some more details then I might be able to find a better fit. 

    Does the customer have any other parameters such as the gain of the system? Any noise requirements?

    Also is there a specific package that's needed? Motor drive applications can be very space constrained so something like a RUC package (X2QFN) might be more appealing to the customer than an SOIC package, both of which the TLV9154 has. 

    Best Regards,

    Robert Clifton