Part Number: OPA541
Other Parts Discussed in Thread: TINA-TI, OPA549
Hi,
As per the information from the datasheets, I was using OPA 541 in the Single Supply configuration (+36V and GND). But in order to get the proper output, I need to apply biasing voltage at the input terminals of the Op-amp. Especially in the non-inverting configuration, I need t to apply -5V (V2) in the inverting pin. If I'm using a -5V in the circuit, then there is no advantage in going with the single supply configuration. Any solution to replace this -5V.
Thanks in advance.