Hi
I have a customer user THS6214,Is the 21mA current of Full Bias Mode only the current of each channel?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
That is correct, it would be the amount of current consumption for each channel or port. So the entire IC, if you are powering both channels, will use double the amount of current listed.
Thank you,
Sima