Part Number: LMV981-N
Other Parts Discussed in Thread: LM358
Hi team,
My customer designed this device and met application problem need BU's support. Thanks
1.
When the input voltage of LMV981_+IN is below 20mv, the response time of output LMV981_OUT becomes longer.
8us@20mv, 24us@6mv, 40us@3mv.
Is this situation caused by the characteristics of the IC itself?
Any suggestions for improvement of this kind of abnormality?
2.
The given Ton from shutdown in the datasheet is typ 12.5us@2.7v. ).
Please also provide the maximum and minimum values of Ton from shutdown@3.3v
3.
When LMV981_+IN input voltage ≤ VOS max (4.0mV),
Does it affect LMV981_IN- output accuracy and NOISE?
If it is affected, what are the suggestions for improvement?