Part Number: INA250
Hello,
I use TI WEB's Current sense amplifier error analysis to calculate the variability of INA250A2.
So I would like to ask you a question.
As a result calculated by the tool, in the case of 3.675A, Total Error was output as 1.408%.
(question 1)
In this case, how should I calculate the VOUT of INA250?
Does the following content match?
Since VOUT = ILOAD × GAIN + REF,
ILOAD x GAIN x 1.01408 ⇒ Device MAX variation
ILOAD x GAIN x 0.98592 ⇒ Device MIN variation
(Question 2)
Is the operating temperature of the tool the ambient temperature or the package temperature?
(Question 3)
Since this device has a built-in resistor, I don't think it is necessary to set the Ideal shunt resistor item, but is it correct?
In this case, is the resistance variation reflected in the Total Error?
Best regards,