Part Number: THS4513
Other Parts Discussed in Thread: , ASH
Hello,
I am having the circuit same as Figure 80 in the datasheet. My supply input is 1.5Vp-p. VS+ is 5VDC,VS- is GND. Trying to make the differential to single ended signal with offset of +2.5VDC.
Output signal clips at 2.5 volt and can't get higher than 2.8V.
Simulation is giving me the same result. I can make this happen only if I connect the VS- to the -5VDC.
I am using the THS4513 commercial grade for now but eventually we will use the THS4513-SP.
Thanks
Ash