Other Parts Discussed in Thread: OPA858
Hi Team,
Our customer is looking for the two modules with the characteristics below. However, upon checking our product lines, it seems we don't have these types of devices. Can you please confirm? I included the D flip-flop just to show the customer's application but I understand that we don't have D flip-flops that could operate at GHz frequency.
8-12 GHz tunable thresholder (like a comparator whose threshold voltage is tunable and at the output passes the signal above the threshold limit)
8-12 GHz D-flip flop (high-speed flip flop to create longer duration pulses based on the input signal, which is the output of threshold)
2. Can I use it to broaden my pulse duration? Meaning that by inserting a pulse of 0.1 ns duration I can get another pulse at the output with 10 ns duration
Due to their speed, I'm looking for an LGA package device or IC which is already mounted into an evaluation board and I just need to plug the voltages with an SMA connector into such component.



Danilo