Part Number: LOG114EVM
Other Parts Discussed in Thread: LOG114,
On the front page of the log114 datasheet is a schematic for a log-ratio amplifier using current from two photodiodes. This is the circuit I would like to test. However, there seems to be only 1 input and a fixed reference current in the manual for the log114EVM evaluation module. Is there any way of testing a log-ratio amplification circuit on this board?
Also, the log102 data sheet shows bandwidth for a range of input currents, but the log114 data sheet has only a gain bandwidth product of 50 MHz at 1 uA. Is there any information about the bandwidth of the log amplifier for different currents? Thanks.