Hi team,
I have a question about the gain of AMC1301.
I'm testing the AMC1301 and there are unclear points that are not mentioned in the datasheet.
We tested the parts individually, and measured the gain from the relationship between the input voltage and the output voltage.
When VDD1 is turned on and off, gain changes.
The voltage value of VDD1 has not changed.
The amount of change in gain is about 40-50ppm.
The gain takes two values, and it occurs randomly and discretely when VDD1 is turned on and off.
Do you have any knowledge?
How can I make gain have the same value even if vdd1 is turned on and off repeatedly?
Best regards,
Teruhito Ishibashi