Other Parts Discussed in Thread: JFE150,
Could the "Input gate current" specification in the rev A datasheet a typo?
VDS = 0 V,
VGS = –30 V
TA = 25°C
IG = 0.2 pA typ / 60 pA max? <-- could the unit be nA instead of pA?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As far as I can see, rev. A has not yet been published. (The first revision is SLPS730 without a suffix.)
The JFE150 datasheet mentions the test condition "VGS = −0.7 V" for this value. This gate voltage is near the best case (see figure 6-7), so pA is correct.
Hello,
+/- 60 pA is correct for room temperature, the JFETs and clamps connected to the gate both exhibit very low leakage.
Please let me know any more questions about the JFE2140!
Best Regards,
Mike