Part Number: OPA857EVM-978
Other Parts Discussed in Thread: OPA857,
To evaluate the OPA857 I purchased a OPA857EVM-978 board but I am a bit confused by the output configuration of the board. First of all my board had R15 installed and not R14. So there was no output at VOUTP but there was at VOUTN. Not a big deal but took me some time to figure out.
After shining some light onto the PIN photodiode (Hamamatsu S5972) I was wondering about the low output level. I could clearly see my pulses but the amplifier was saturating at about 30mV peak (with 3.3V VCC). Measuring with a probe directly at R6 and R7 revealed a voltage swing of around 500mV. What is the purpose of R6 and R7? It is increasing the output load of the amplifier while sacrificing some gain?
Is it safe to short R6,R7 and remove R8? The two 25 Ohms in series with the output pins should make up for a total of 50 Ohms differential. Which the 1:1 BALUN will transform to 50 Ohms single ended. Do I miss something here?
Thank you,Tobias