Part Number: OPA564
Other Parts Discussed in Thread: TINA-TI
Hi everyone,
I'm using the OPA564 to feed an inductive load of 2 ohms and 47µH at 100 kHz.
My input signal is a sin wave with a 700mV amplitude. I have a gain of about 4 so I have an output of about 3V to feed my load.
At 100 kHz, my load exhibits about 30 ohms of inductive reactance. That means that the maximum current travelling through the coil should be 100mA.
But I have a problem : the power supply indicates that more than 300 mA are delivered to the circuit.
A precision : I did not make a thermal pad. It was just a test for the OPA564 (just to check the good functionning of my circuit). I was thinking that with 100mA, the thermal problematics would not appear, but the thermal protection goes on and off in a cyclic way.
So the question is : do you have an idea why the current is too high related to what was expected? Could it be due to the absence of thermal pad?
Thank you in advance
Sylvain