I am looking for a PIEZO driver/ amplifier series from TI. I was first looking at TREK products, but got some recommendation that TI products are much reasonable.
www.piezodrive.com/.../
- Following link is the driver/amplifier which can be used in experiments.(adjustable parameters)
Can anybody advise me of TI products to drive/amplify the below type piezo?
1.Tube type :
tube c255 o12 i10 L13 eAg (000068893),
2.DISC type :
disc c255 o10 t2 eAg (PRYY+0372),
3.PLATE type :
plate c255 x10 y10 t2 wCuNi (000041652),
4.RING type :
ring c255 o9 i4 t2 eAg (000059262),
The piezo was purchased in PI.
Looking forward for answers. Thanks!