Part Number: OPA548
Other Parts Discussed in Thread: OPA192, CSD18540Q5B
Hi,
We are trying to design a current amplifier with the following requirements:
- An AC signal, isn't necessarily a sinusoidal.
- 10V <=Vout<=16V @ 15HZ - 15KHZ (or as close to this full frequency range as possible).
-Our current demand is 30A max.
The simulation results indicate that the design might be able to work with the proper output capacitance compensation (the circuit is supposed to drive one of our boards which has a high input capacitance, that I added to the output in the attached simulation model).
The Data Sheet of OPA548 doesn't specify the output resistance of this op-amp and I'm not sure that the simulation takes into account the exact output resistance. Even if it does, I prefer not to guess the exact capacitor and resistor that should be added as an in-loop compensation.
can you please suggest the compensation values for this circuit or provide a PN of more suitable op-amp for our design?
Thanks!
Anna