Part Number: INA237
Other Parts Discussed in Thread: INA226, INA238
Hello,I have tried two types of INA237。they are INA237AIDGSR and INA237AQDGSRQ1,and I connected it with STM32, below is the schematic

And I found it was really weird that the register value didnot match the datasheet,below is the register value I had read。

However, I also tried to use INA226 to replace the INA237(pin-pin),and ramained the code and schematic unchanged,then I can read the right value 。
I dont know why。。。。

,yellow line is SDA,red is SCL,the test point was on the pin.2 and pin.3 of ADUM1250。
at this time ,the scope shots were almost the same ,the 0.8-1V stage of low level still existed,and also exceed the VIL threshold of INA238。
,then,