Part Number: TLV7041
Hi,
From the datasheet, Vin spec is VCC + 0.1V, and in my design there is possibility of Vin supply available first before VCC,.
1) Is disconnecting the ground before VCC available able to protect the op amp? Something like below. Without the ground reference, will Vin damage the part?

2) With the above configuration, without VCC and ground, with Vin (at pin 3)=5V, will i see any voltage at output pin 1?
Thanks!