This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV333: Electrical Characteristics

Part Number: TLV333


Hi,

Good day. Can you please help us with the below information needed for TLV333.

1.Output voltage High
2.Differential input voltage value

Thank you.


Regards,

Cedrick

  • The TLV333 maximum linear output voltage swing is specified in the AOL condition to be 100 mV from the rail:  (V+) -100mV, while typical non-linear output swing (resulting in large increase in the input offset voltage) is within 30mV - see below.

    TLV333 is a zero-drift op amp with auto-zero self-calibration, which should NOT be used as a comparator by pulling the input terminals apart.  Taking the inputs more than 0.5V apart will forward bias one of parasitic diodes inside the front-end input stage as shown below.  This may lead to TLV333 damage unless the input current is limited to 10mA or less.

  • Hi Mark,

    Thank you.

    Our customer has an additional question.  They also need Absolute maximum Differential input voltage value.

    Regards,

    Cedrick

  • Cedrick,

    The maximum differential input voltage may be back-calculated based on the information given above.  Since there is total of 20kohm between the input terminal, as shown in Fig 20, the max Vin_diff=20k*10mA=200V.  Just please be aware that exposure to absolute maximum rated conditions for extended periods of time may affect device reliability - see below.