Part Number: INA2191
for the package YBJ0012 the body dimensions are missing
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA2191
for the package YBJ0012 the body dimensions are missing
Laura,
Thank you for bringing this to our attention! I have reached out to the packaging team to request that the legend be added to the drawing. The typical values are present on the first page of the datasheet, but I will respond once I have this information for min/max info as well.

Laura,
I am still working with our web team to get the document rectified, but I have received the values that should be populated here in the mean time.
D max: 1.558mm, D min: 1.498mm
E max: 1.2mm, E min: 1.14mm