Other Parts Discussed in Thread: OPA191
We manufacture a piece of military aircraft test equipment that uses the OPA111BM which is discontinued. The op amp is used in a test instrument that measures the AC capacitance and insulation resistance (megger) of the sensing probes in a fuel quantity system..The OPA445BM appears to be a suitable candidate for replacement, however, we do not get the same (insufficient) response from the external offset trim when we installed the OPA445 in the circuits.
We use 5 of the op amps on three different circuit boards in the tester. Some circuits use the trim leads and some do not. On the ones that do not use the trim leads, the OPA445 seems to work the same as the OPA111. On the circuits that use the trim leads, we do not have enough trim authority (range).
Per the data sheet, the OPA111BM has a 10K and two 2K resistors in each internal trim circuit. What are the resistance values for the resisters in the OPA445BM trim circuits? Can you provide a schematic of the internal trim circuits of the OPA445BM? The trim circuit in our circuit is the same as that shown in Figure 2 of the OPA445 data sheet SBOS156B, including the recommended 100K trim pot.
Below is a section of our megger circuit.