This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLE2024B

Other Parts Discussed in Thread: TLE2024

Hi, I am working on an existing design where we are experiencing some opamp power interrup problems.

During a power interrupt some times the op amp is no longer behaving correctly. The datasheet indicates that the tle2024 is supposed to operate down to 2V is that correct? I think the op amp begins misbehaving at 3 to 4 V.

What happen if the output of the op amp is shorted for a few hundred milliseconds? Can it be damaged? The datasheet indicates that it is OK to short the output.

What is the common mode input voltage range of the op amp at +/-12V at +/-5V and at +/-2V?

 

Thank youy