Other Parts Discussed in Thread: LMV358A, LM358B, TLV9002, LM358LV, TLV9302
Hi,
The customer chose TL022 instead of NJM022M, but is using it with a single power supply.
I think the headroom is the same (up to 3V, TYP 2V) when using this product with a single 5V power supply, is that correct?
NJM022M is the same as TL022 in the data sheet, but it seems to be about 1V in actual use.
Is there similar data for TL022?
If not, I would choose RRO's OPAMP.
Best regards,
Hiroshi