Part Number: INA240
Other Parts Discussed in Thread: INA293
Hi,
Our customer likes the INA240 for their FOC motor application but they have a tight space constraint. They also care about EMI/noise as well.
Can you recommend a few alternatives that are smaller in footprint size?
Few other details...two sets of parameters:
Vcc = 3.3V, Vbus = 48V, Imax = 20A, PWM = 45kHz.
Vcc = 3.3V, Vbus = 24V, Imax = 5A, PWM = 45kHz.
-Kelvin