Part Number: THS4541
Hi Team,
Good day! I am posting this in behalf of the customer.
I have shared the full details of the inquiry here:
I am using THS4541 differential amplifier to amplify a very low-voltage signal. The max. achieved gain of THS4541 is 14 V/V, however I need a higher voltage gain. Can I use two THS4541 in serial (cascaded) to achieve a higher gain factor? I am planning to connect the differential output of the first THS4541 to the differential input of the second THS4541 and to arrange for gain 10 V/V both. In that case, can I achieve 100 V/V gain (10*10) at the output of the second THS4541 according to the input of the first THS4541? Please could you recommend/provide some technical details for getting a higher gain factor?
Best regards,
Jonathan