Part Number: OPA698
Hi I have a circuit comprising OPA698 with gain x2 with input +/- 1.5V and limiting +/-0.3V and am seeing settling time to 6mV (2%) is out past 100nS. From the datasheet it says 2nS for 2x overdrive with clamp levels set to +/-2V. I'm trying to understand how to best optimize this part for my application. (I originally tried with x5 and x10 gains but this was even slower so thought x2 gain might solve issue).Do you have any numbers for higher levels of overdrive, or with lower clamp voltages ?