Other Parts Discussed in Thread: ADS1299, OPA376, TLV376, OPA387, OPA391, OPA397, OPA392
Hello,
we are working on product development of EEG device. we have choosen ADS1299 for the front end EEG capture. right now we have to design an active electrode for EEG, in which we are going to use DRY electrodes, so have Active electrode is best option. for that, we were unable to find any reference designs. could you please suggest us the best and available opamp parts for using in the design which ever is compatible with the input of the ADS1299 . we are bit confused like whether we should use precision amplifiers/general opamps or instrumentation opamps.which should be considered for this application. we might need a very lower offset, high CMMR, low noise ampliers which can work using -2.5 to +2.5 Dual polarity supply. please suggest us part numbers and if any reference designs available for active eeg electrode please share it. and more over the size should be smaller as possible as entire active electrode circuit has to be fit in a <10mm dia PCB. Thank you
with regards
Dr.N.Chandra Sekhar,phd