Part Number: LMH6553
In the data sheet, page 4, the maximum VCLAMP voltage is specified as VCM + 2.0V. Note 7 specifies that exceeding the limits could result in excessive device current.
However, the test conditions above the table specify VCM = 0V and VCLAMP = 3V (for the +/-5V condition).
So, should the device be operated with VCLAMP > VCM + 2.0? If so, what is the actual limit?
Best regards,
Eamon Egan