This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA364: OPA364

Part Number: OPA364

 a component after being mounted on PCB failed in ICCT test 

供应商:Mouser

PO:633730

order Qty:750

DC:2003

  • Gary,

    Please describe the setup used for the ICCT test on the OPA364 pins. Also provide test limits.

  • Hey Garry,

    Could you please provide some additional information as far as the failure for the device? What is the application/circuit this is being used in (a schematic would be helpful). Additionally between which pins of the device are you seeing short circuits?

    Best,
    Jerry 

  • Normal setup ,actual reading(measure value) for passed N2  and test limits as below( the details please refer to the test log  as attached fileICT testlog(line 972&973).xlsm:

    Component   Result   Type  Measure Val  Low Limit  High Limit
    N2%OUTPUT_1_HIGH   PASS   A-MEA  2.000441 1.5 2.5
    N2%OUTPUT_1_LOW   PASS   A-MEA   102.106500 m   50.000000 m   150.000000 m 
  • HI Jerry

    please see the schematic as belows:

    We don't kown how to identify which two pins the short occurs on ,so need send the defective component to you for further anaysis.

    Thanks

    Garry

  • Hi Ron

    In addition,please refer to the ICT failed report as below or  attached file.

    ----------------------------------------
    Shorts Report for "shorts".
    Thu Nov 18 15:44:47 2021
    402263411981
    Board Version: **BASE**
    ----------------------------------------
    Short #1, Thresh 1000, Delay 50us Ohms
    From: N2 20417 2
    To: H_MUX_ADC3_N 20237 4
    MAIN__AI_ADC___1N2856 20504 4
    MAIN__SI_CHK___1N2087 20318 3
    Total of 4 nodes, Message is: None.
    ------End, 1 Problem Reported-----------
    ========================================
    Customer: Neways
    Test Result: FAILED ICT
    Assy #: 606071001 Rev. A0.0
    Serial #: 000000000130747429
    ========================================

     

    ----------------------------------------
    Shorts Report for "shorts".
    Thu Nov 18 15:44:47 2021
    402263411981
    Board Version:  **BASE**
    ----------------------------------------
    Short #1, Thresh 1000, Delay 50us   Ohms
    From: N2                      20417    2
    To:   H_MUX_ADC3_N            20237    4
          MAIN__AI_ADC___1N2856   20504    4
          MAIN__SI_CHK___1N2087   20318    3
    Total of 4 nodes, Message is:  None.
    ------End, 1 Problem Reported-----------
    ========================================
            Customer:  Neways
    Test Result: FAILED ICT
    Assy #: 606071001 Rev. A0.0
    Serial #: 000000000130747429
    ========================================
    

  • Garry,

    The powered tests provided a great 2V and 0.1V, so the op amp is working fine. The OPA364 has many specified parameters, but none are provided for power off tests such as "shorts".  Without knowing the exact pins and applied signal, I can't determine if the issue is device or ICT test setup or limits. 

    If you still want FA, follow the steps below.  

    On request concerning suspect non-conforming TI material to visit TI portal for Customer Product Return (CPR):
    www.ti.com/support-quality/resources/customer-returns.html and to follow TI guidelines for returns www.ti.com/lit/sprac01.
    On general questions about TI quality please visit www.ti.com/quality.