Part Number: LMV881
Hello TI experts,
I want to know about the shutdown function of LMV881.
on page 13in the datasheet, I can see the description as below ;
---
To conserve battery life in portable applications, the LMV881 can be disabled when the shutdown pin voltage is pulled low. The shutdown pin is designed for 1.8V logic levels, with thresholds independent of total supply voltage.
---
then can't I use 3.3V or 5V as a control of shutdown pin?
cause my customer use only 3.3V and 5V for their device.
please check this issue. Thanks.
Best regards,
Chase