Other Parts Discussed in Thread: TPS61085, LM2623
Hi,
Is there any low cost versions for TPS61085?
Thanks.
Vito
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear,
Here is the spec. required for the project,
Input voltage:2.5V ~6V.
Output voltage: 8V
Output current:>200mA
Oscillation frequency: <1MHz.
Over current protection.
Thermal shutdown.
Any suggestion?
Thanks,
Hi Vito,
We don't have cost down version for TPS61085. You may consider LM2623 with lower cost.