Other Parts Discussed in Thread: TPS61085, LM2623
Hi,
Is there any low cost versions for TPS61085?
Thanks.
Vito
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Not with exactly the same parameters.
What parameters do you actually need?
Dear,
Here is the spec. required for the project,
Input voltage:2.5V ~6V.
Output voltage: 8V
Output current:>200mA
Oscillation frequency: <1MHz.
Over current protection.
Thermal shutdown.
Any suggestion?
Thanks,
Hi Vito,
We don't have cost down version for TPS61085. You may consider LM2623 with lower cost.