Part Number: VCA2615
Hello all,
I use VCA2615 in ultrasonic application.
On the page 18 of Data Sheet
Table 5. shows codes for Feedback Resistor Settings.
I have come across that setting any code other than
'1111' (Open) causes a significant increase in noise.
For example, for code = '1111', input termination Rl=0, amplifier gain = 52dB
(about 16dB for LNA with a single ended input plus 36dB for VCA)
output noise voltage
Uout,rms=1.2mV
For code = '0000'
Uout,rms=3.59mV
For code = '0001'
Uout,rms=3.57mV
..................
For code = '1101'
Uout,rms=2.44mV
For code = '1110'
Uout,rms=2.14mV
Please answer two questions:
1) Why is this happening?
2) What is FEEDBACK RESISTOR for code '1111' (Open) ?
Thank you,
Best regards,
Viktor.pulsarvictor2003@gmail.com