This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sinusoidal Current Source for Inductive Load

Dear TI Team,

We need to design a sinusoidal current source with provision to tune frequency (1k to 10 k), current (1-200 mA) which can drive a variable load in which inductance can vary from 1 to 25 mH, and load resistance 1-200 ohm.

Once the current is set, it should be steady within 1mA for the entire range of load.  

I request the team to please suggest an OPAMP which can drive the 200mA at maximum load value i.e. 200 ohm = R, and Xl = 25mH @ 10KHz. 

Just saw some circuit here but I am still looking for some OPAMP or a circuit based on that which can handle the compliance voltage at rated maximum current and maximum load value (impedance)

https://www.ti.com/lit/ds/symlink/opa454.pdf?ts=1642646532018&ref_url=https%253A%252F%252Fwww.google.com%252F

Can someone please help in this regard?