Part Number: TLV3501
Hi Team,
Customer is trying to characterize the Tpd vs factors.
Customer uses triangular waveform at different freq to compare and found Tpd difference in TINA simulation vs real test.
Before helping customer to work out a meaningful data, I want to double verify if my understanding is correct, thanks for help.
1. Tpd mainly depends on overdrive voltage btw input pins? My feeling is that it's difficult to connects existing Tpd data with a moving signal at either IN+ or IN-, overdrive vs Tpd chart is more about DC voltage vs output delay, so is there any method we can roughly determine Tpd in a triangular waveform (for example 50kHz and 5kHz) with existing chart as below?
2. CMRR can be used to calculate how much Vos error is produced based on common mode voltage being applied to input pins, [IN(+) - IN(-)] / 2 ?
for example if CMRR = 70dB, common mode 1V will result in 316uV offset, considering TLV350x 5V device, the working input range is small, so CMRR should be a small factor to Tpd, correct?
Thanks!
Andrew