Other Parts Discussed in Thread: OPA301,
Hi Team,
I plan to buy a ISO224EVM borad for test, I have some questions need your help, thanks in advance.
1. If VDD1 is 5V, can analog input be 12V and higher than VDD1?
2. if VDD1 is generated from VDD2, analog input ground needs to be connected with GND1, for example, analog input is devided from 400VDC, then ground of 400VDC should connect with GND1, right?
3. The Voltage signal I want to measure is 10us pulse, I simulated the circuit with TINA , the amplier on EVM board looks response is too slow, I changed to OPA301, but output has distortion, could you help have a look what the reason, thanks.