Part Number: OPA330
This part is configured as a buffer using OPA330AIYFFR.
When 0.5V is applied to the input I measure 2.2V, the correct value should be close to 0.5V. Please help to verify if there is an issue with the part.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA330
This part is configured as a buffer using OPA330AIYFFR.
When 0.5V is applied to the input I measure 2.2V, the correct value should be close to 0.5V. Please help to verify if there is an issue with the part.
Hello Kai,
Found the issue there was a damage part on the PCB. Fractured part.... you can close out
Hi David,
Thanks for the confirmation!
It will be quicker to provide us with a schematic and load conditions. As you did, you may contact our FAE and they are able to reach us directly via email or phone call etc..
Thanks,
Raymond