Part Number: INA188
Other Parts Discussed in Thread: INA826, INA818
Hi,
the schematic is as below: INA188 is powered by single 5V.
pin 5 REF=0.283V, a thermocoupler is connected to J2.
When the input (IN+)-(IN-)=0, the output is 0.255V, which is supposed to be 0.255V.
I've no idea why there is such big error.