Part Number: TRF37B75
Hi Team,
Customer needs to select RF amplifiers. He has some questions about the selection of RF choke inductance parameters:
1. How to determine the inductance value of choke inductance? Only 100nh is provided in the manual. Is there a specific basis for the selection of sense values? Is it related to the selected RF amplifier model?
2. Due to the high frequency of the inductors used in RF, it is generally considered to use special RF inductors such as coilcraft manufacturers. When choosing this kind of inductor, he will pay attention to the indicator of self-resonant frequency. However, it is difficult for TRF37B75 or similar devices to reach 100nh inductance self-resonant frequency in the 4000mhz frequency band to 4000m. 100nh inductors can only do less than 1G. How should the self-resonant frequency srf of the 100nh inductor be selected?
3. The choke inductor is mainly to prevent the signal from passing to the DC terminal. When paying attention to the impedance of the working frequency band of the inductor, should the impedance of the working frequency band of the inductor be as high as possible?
Thanks,
Annie