This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BUF634 - connection of SO-8 NC pins for heat sinking?

Other Parts Discussed in Thread: BUF634

The BUF634 in SO-8 is very nice (if a little pricey), but the NC pin usage is unclear. For keeping the die temperature down, can/should I connect the NC pins to GND, or to V- as in the TO-220 & DPAK??

Thx!

  • Alexander,

    The "NC" pins on the SO-8 package are not connected internally. You can connect them to any convenient node or they can be left unconnected. To increase heat dissipation, the landing pad area and connection leading from it should be maximized. Area is the key, not where they are electrically connected.

    Regards, Bruce.