Part Number: OPA145
Other Parts Discussed in Thread: STRIKE, OPA627
OPA145 datasheet specifies that the device pins feature ESD ruggedness according to 2 kV Human body model.
1) Does this apply while the amplifier is powered up ?
2) Does this mean that the input protection diodes survive direct exposure to a 2 kV, 100 pF, 1.5 kOhm strike without additional components? Obviously the resulting current of more than 1 A for about 50 ns is way above the Absolute Maximum Rating of 10 mA.
Background: I have an application where the non-inverting input of the opa145 is directly exposed to a device interface and will be subjected to 61000-4 testing for ESD and EFT. *Of course*, I will provide additional protection, but it is a *HUGE difference* if this additional protection has to limit the 50-ns-transient current to something like several 100 mA or to a few mA.
Kind regards!