Hi,
Could you please let us know the output pin status on LM2903BIDR under Vcc<2V.
My customer considers the following circuit.
LM2903BIDR's pin condition is as follows:
- Vcc : 5V line from DC/DC
- IN+ : Divided resisters on 5V line from DC/DC
- IN- : LOW (Pull-down) during 5V power-up
- OUT : connected with /SHDN (internal pull-up on 2.7V)
Under the above case during power-up on 5V line, after Vcc>2V, output of LM2903B is open and /SHDN pin is 2.7V. How about Vcc from power-up (0V) to 2V? Is it possible to output low from LM2903B under Vcc<2.0V condition? Please advise us.
We understand LM2903B is unknown status under Vcc<2.0V. However if it is possible to output low on LM2903B, this system can not wake up, because TPS26631 is shutdown and power is OFF if /SHDN is low (under 0.8V). So please support us.
Thanks and best regards,
M.HATTORI.