Other Parts Discussed in Thread: AMC1301, AMC1200, TLV170, OPA350, TLV6001, AMC1300, AMC1350, AMC1351
Dear TI team,
Good evening.
We are using AMC1100 for AC voltage sensing(0-270V),DC voltage sensing(300V DC and 600V DC) and AC current sensing(24A).
1.Can we use AMC1100 in AC voltage sensing and AC current sensing and is this good choice?
2.Can we use AMC1100 in DC voltage sensing(600VDC)?
In one of TI application note ,I found these lines while comparing AMC1100,AMC1200 and AMC1301,
"The AMC1100 or AMC1200 provide basic isolation with similar performance to the AMC1301 at a lower price point.For applications requiring a bipolar output option,the TLV170 is an excellent choice."
Based on above we have few questions:
1.Can we replace AMC1100 for better performance with any of above differential isolated amplifiers?
2.As pin out are same,can we replace AMC1100 with AMC1301 or AMC1200?Any modifications required?
3.For single ended ADC,we are using OPA350 op amp ,but in application its said to use TLV170?is opa350 opamp ok?
or we need to use TLV6001 or TLV170?
Kindly check and clarify.
Thank you,
Caliber