This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9032: Datasheet Table question

Part Number: TLV9032

Hi TI,

Looking at the datasheet (the version found here at least: https://www.ti.com/lit/ds/symlink/tlv9032-q1.pdf) I noticed that table 6.6 and table 6.8 appear to be identical except for two PSRR entries in table 6.8 which do not appear in table 6.6.  The conditions noted right under the "6.6 Electrical Characteristics" and "6.8 Electrical Characteristics" are identical, and as far as I could tell the parameters, test conditions, min/typ/max and units (i.e. all the data) in the table are identical.  If this is true, what is the purpose of 6.6?  Are there actually two different conditions (e.g. one is for 3.3V supply voltage and one is for 5V where both are accidentally labeled as 5V)? or is it just an accidental duplication.

Thanks,

Max